Is there any port for an NXP Cortex evaluation board that support the .Net Micro Framework? Is NXP or any third party supporting the .NET Micro Framework?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is there any port for an NXP Cortex evaluation board that support the .Net Micro Framework? Is NXP or any third party supporting the .NET Micro Framework?

1,912件の閲覧回数
lpcware-support
Senior Contributor I

The open source .NET Micro Framework requires a device with at least 256kB of flash and 64kB of RAM. A device with an external memory bus for memory expansion is highly recommended.

Please visit http://www.netmf.com/ for details on the .NET

There are two evaluation boards that support .NET MF:

* Embedded Artists EA_LPC2478 (NXP LPC2478 processor)

* Phytec Rapid Development Kit PCM023 (NXP LPC2294 processor)

ラベル(2)
タグ(2)
0 件の賞賛
返信
1 返信

1,702件の閲覧回数
lpcware-support
Senior Contributor I

#1 Submitted by rocketdawg on Wed, 2013-10-02 16:28.

the Bambino 200 is based on a LPC4330 and it supports NETMF

0 件の賞賛
返信