Is there any port for an NXP Cortex evaluation board that support the .Net Micro Framework? Is NXP or any third party supporting the .NET Micro Framework?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there any port for an NXP Cortex evaluation board that support the .Net Micro Framework? Is NXP or any third party supporting the .NET Micro Framework?

1,915 Views
lpcware-support
Senior Contributor I

The open source .NET Micro Framework requires a device with at least 256kB of flash and 64kB of RAM. A device with an external memory bus for memory expansion is highly recommended.

Please visit http://www.netmf.com/ for details on the .NET

There are two evaluation boards that support .NET MF:

* Embedded Artists EA_LPC2478 (NXP LPC2478 processor)

* Phytec Rapid Development Kit PCM023 (NXP LPC2294 processor)

Labels (2)
Tags (2)
0 Kudos
Reply
1 Reply

1,705 Views
lpcware-support
Senior Contributor I

#1 Submitted by rocketdawg on Wed, 2013-10-02 16:28.

the Bambino 200 is based on a LPC4330 and it supports NETMF

0 Kudos
Reply