Is the frame buffer inside the 1788 or in an external device?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Is the frame buffer inside the 1788 or in an external device?

1,615 次查看
lpcware-support
Senior Contributor I

The frame buffer can be in any contiguous block of memory. This could include a block of internal SRAM or in external SDRAM or SRAM. Usually, the frame buffer storage requirement (depends on LCD resolution and colors) is too large to fit in internal SRAM and external SDRAM is used.

标签 (2)
标记 (2)
0 项奖励
回复
0 回复数