Is the frame buffer inside the 1788 or in an external device?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is the frame buffer inside the 1788 or in an external device?

1,284件の閲覧回数
lpcware-support
Senior Contributor I

The frame buffer can be in any contiguous block of memory. This could include a block of internal SRAM or in external SDRAM or SRAM. Usually, the frame buffer storage requirement (depends on LCD resolution and colors) is too large to fit in internal SRAM and external SDRAM is used.

ラベル(2)
タグ(2)
0 件の賞賛
返信
0 返答(返信)