Is it possible to use both the USB device and Ethernet on LPC1758, since MDIO and USB_connect are shared? Is there a possible workaround?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Is it possible to use both the USB device and Ethernet on LPC1758, since MDIO and USB_connect are shared? Is there a possible workaround?

1,830 次查看
lpcware-support
Senior Contributor I

The Ethernet PHY configuration is a one-time event. Once the configuration has been completed using MDIO and MCLK, these pins will no longer be required. It will then be possible to switch the pin function to USB.

Another option is to use Ethernet MII Management (MDIO) using software. This is described in Application note AN10859.

http://cache.nxp.com/documents/software/AN10859.zip

If MDIO is implemented in software, there will be no need to share pins between USB and Ethernet.

标签 (3)
标记 (3)
0 项奖励
回复
0 回复数