Is it possible to sample two analog signals at the same time on a Cortex-M3 device?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is it possible to sample two analog signals at the same time on a Cortex-M3 device?

2,129件の閲覧回数
lpcware-support
Senior Contributor I

The LPC13xx and LPC17xx families have a single ADC and sample-and-hold, so sampling multiple signals at the same time is not possible, unless an external sample-and-hold circuit is utilized.

The LPC18xx microcontrollers are a high performance Cortex-M3 family that has two ADCs, so it would be possible to sample multiple signals at the same time with these devices. The LPC43xx Cortex-M4 devices would also be an option since they also contain multiple ADCs.

ラベル(7)
0 件の賞賛
返信
0 返答(返信)