How can I test the CAN peripheral and driver without a CAN transceiver and CAN bus connected?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How can I test the CAN peripheral and driver without a CAN transceiver and CAN bus connected?

5,746件の閲覧回数
lpcware
NXP Employee
NXP Employee

Use the internal loopback feature of the CAN controller. This allows the controller to receive what it transmits without the bus being used. Typically this mode is enabled by setting a bit in the control register before enabling the CAN controller.

"FAQ contribution from Embedded Systems Academy, experts in CAN bus. For more information visit www.esacademy.com"

ラベル(1)
  • CAN

タグ(1)
0 件の賞賛
返信
0 返答(返信)