Does emWin support touch panels?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does emWin support touch panels?

1,746件の閲覧回数
lpcware-support
Senior Contributor I

Touch screen support for analog touch panels is available, including a low level driver, which handles the analog input (from an 8 bit or better AD-converter), debouncing and calibration of the touch screen. The window manager deals with touch messages and widgets such as button objects. It takes no more than one line of code to create a button or another widget, which then automatically handles touch messages and reacts accordingly. emWin also supports mouse and keyboard inputs.

The touch screen simulation is integrated into the regular emWin simulation. Mouse events are used to simulate the touch screen. The simulation can be used to write the user interface of your application and can be sent as a simple .exe files to anybody for discussion, demonstration or verification.

ラベル(2)
タグ(2)
0 件の賞賛
返信
0 返答(返信)