Does emWin include a simulator which graphic designer can design without evaluation board?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does emWin include a simulator which graphic designer can design without evaluation board?

1,828 Views
lpcware-support
Senior Contributor I

The PC simulation of emWin allows you to compile the same "C" source on your Windows PC using a native (typically Microsoft) compiler and create an executable for your own application. The resulting executable can be easily sent via email. With the simulator, you can design the user interface on your PC (no need for hardware!), debug your user interface program, and create demos of your application, which can be used to discuss the user interface.

Labels (2)
Tags (2)
0 Kudos
Reply
0 Replies