Can the RTC output be used for PLL0 input?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can the RTC output be used for PLL0 input?

1,415 次查看
lpcware-support
Senior Contributor I

Yes, the RTC oscillator can be used as a clock source for PLL0, however, when using PLL0 to drive the USB controller, the RTC cannot be used as the clock source. The reason it cannot be used for driving the USB controller is that an FREF less than 100 kHz will need to be used, and this causes a high jitter, which can cause a problem for PLL0.

标签 (1)
标记 (1)
0 项奖励
回复
0 回复数