where is the mcg_config_t declaration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

where is the mcg_config_t declaration

5,583 Views
PO220
Contributor IV

Hi

I' use KDS 3.2 with SDKv2.0 and 2.2 since they exist

Now I'm trying to make a new project with KSDKv2.3 for KL27Z128

File->new->kinetis SDK v2.x Project

I select KL27Z128, All drivers, Freertos...and there surprise :

@unknown type name 'mcg_config_t'    clock_config.h   (extern const mcg_config_t mcgConfig_BOARD_BootClockRUN;)

But where is this definition ? (A search of the entire folder SDK_2.3.0_MKL27Z128xxx4 only finds mcg_config_t in two files  clock_config.h and clock_config.c ; no definition of  mcg_config_t !?! )

Thanks in advance, I'm totally blocked by this thing

In addition to that with version 2.3 the import of a demo does not work  (no demo proposal in the wizard and import->Existing Projects into Workspace give an invalid project with any source file in project folder   )

It's sad that it's so complicated to create a project or open a demo :-(

Labels (1)
0 Kudos
Reply
8 Replies

5,121 Views
joshuadonaldson
Contributor II

Was there any conclusion made here? The project templates for the kl27z seem to reference mcg_config_t in the latest v2.3.1 sdk but only the mcglite_config_t is present.

Please urgent rectification is required.

0 Kudos
Reply

5,121 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Joshua:

I checked sdkv2.3.1 (SDK_2.3.1_FRDM-KL27Z) and sdkv2.4 , only found the mcglite_config_t, where did you find the mcg_config_t ?

Regards

Daniel

0 Kudos
Reply

5,121 Views
joshuadonaldson
Contributor II

Hi Daniel,

Please check under devices\MKL27Z4\project_template.

clock_config.c should make reference to mcg_config_t here.

Regards,

Joshua.

0 Kudos
Reply

5,121 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Joshua:

The project templates  should reference to mcglite_config_t, maybe there is an errori n SDK2.3.  

Regards

Daniel

0 Kudos
Reply

5,121 Views
joshuadonaldson
Contributor II

You mean an error in SDK 2.3.1. The project templates don't reference

mcglite_config_t.

0 Kudos
Reply

5,121 Views
danielchen
NXP TechSupport
NXP TechSupport

The project templates in new SDK 2.4 use mcglite_config_t.  Not mcg_config_t.

Regards

Daniel

0 Kudos
Reply

5,121 Views
PO220
Contributor IV

I downloaded the SDK version 2.3 for the KL27z64

it compiles well but the structure mcg_config_t is not called! it's mcglite_config_t which is called, as in the old SDK.

what a waste of time !

0 Kudos
Reply

5,121 Views
PO220
Contributor IV

MCUXpresso SDK API Reference Manual: Clock Driver 

no mcg_confi_t struct  here in my folder SDK_2.3.0_MKL27Z128xxx4.

http://mcuxpresso.nxp.com/api_doc/dev/210/fsl__clock_8h.html  (give 404 error)

0 Kudos
Reply