where is fsl_pmc_hal.c file located in KSDK 1.2?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

where is fsl_pmc_hal.c file located in KSDK 1.2?

1,201件の閲覧回数
charlesm00g
Contributor I

I couldn't find fsl_pmc_hal.c file in KSDK 1.2. Is this file missing or replaced with another file?

ラベル(1)
タグ(2)
0 件の賞賛
返信
3 返答(返信)

1,052件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Charles Mao:

I guess the file you are looking for is "fsl_power_manager.c" and it is with the system files in this path:

C:\Freescale\KSDK_1.2.0\platform\system\src\power


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,052件の閲覧回数
charlesm00g
Contributor I

Hi Jorge,

Thanks for your reply. Actually, I'm looking for the same or similar file fsl_pmc_hal.c which was located at  platform\hal\src\pmc in KSDK 1.1.

Charles

0 件の賞賛
返信

1,052件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hello Charles Mao,

header file for fsl_pmc_hal in KSDK 1.2 is located at c:\Freescale\KSDK_1.2.0\platform\hal\inc\

I hope this helps,

Best Regards,

Iva

0 件の賞賛
返信