where is fsl_pmc_hal.c file located in KSDK 1.2?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

where is fsl_pmc_hal.c file located in KSDK 1.2?

1,283 Views
charlesm00g
Contributor I

I couldn't find fsl_pmc_hal.c file in KSDK 1.2. Is this file missing or replaced with another file?

Labels (1)
Tags (2)
0 Kudos
Reply
3 Replies

1,134 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Charles Mao:

I guess the file you are looking for is "fsl_power_manager.c" and it is with the system files in this path:

C:\Freescale\KSDK_1.2.0\platform\system\src\power


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,134 Views
charlesm00g
Contributor I

Hi Jorge,

Thanks for your reply. Actually, I'm looking for the same or similar file fsl_pmc_hal.c which was located at  platform\hal\src\pmc in KSDK 1.1.

Charles

0 Kudos
Reply

1,134 Views
ivadorazinova
NXP Employee
NXP Employee

Hello Charles Mao,

header file for fsl_pmc_hal in KSDK 1.2 is located at c:\Freescale\KSDK_1.2.0\platform\hal\inc\

I hope this helps,

Best Regards,

Iva

0 Kudos
Reply