usb cdc virtual com problem after cable detached and re attached

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

usb cdc virtual com problem after cable detached and re attached

1,225件の閲覧回数
inorman
Contributor III

Hi I was wondering if anyone else has solved this issue when using the virtual com port, this also occurs when RF noise disrupts the usb link. This is using ProcessorExpert with USB virtual com port. and sdk 1.3.

I've read in another thread  How to recover from USB errors, or how to reinitialize USB0 without a full reset? 

that toggle the usb data line pullups should cause the usb device to be re-enumerated, which appears to work fine however I'm unable to send any further data as the terminal programs hungs.

How should the usb comms be shut down cleanly and restarted? 

It would seem the function Start_Transactions returns 0 meaning the re-enumeration hasn't completed successfully.

タグ(2)
0 件の賞賛
返信
0 返答(返信)