trouble reading uart

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

trouble reading uart

2,412件の閲覧回数
josephgundel
Contributor III

I have 2 UARTs I am using on the K02 Board I have.

 

One is set up for DEBUG and it works normal. I can Use Interrupts no problem.

When I configure the 2nd UART, UART1 I cannot read anything out of the port. I cannot use Interrupts as well.

 

Here is my configuration:

 

/*! User configuration structure 0 */

/*! fsl_uart1 configuration structure */

const uart_user_config_t fsl_uart1_InitConfig0 = {

    .baudRate = 115228U,

    .parityMode = kUartParityDisabled,

    .stopBitCount = kUartOneStopBit,

    .bitCountPerChar = kUart8BitsPerChar,

};

 

static uart_status_t uart1_init(void)

{

    uart_status_t status = UART_DRV_Init(FSL_FSL_UART1, &uart1_state, &fsl_uart1_InitConfig0);

    UART_HAL_SetIntMode(g_uartBaseAddr[FSL_FSL_UART1],kUartIntRxDataRegFull,true);

    return status;

}

 

I have tried reading using blocking and also using an Interrupt and It never reads anything. I can transmit out no problem but I cannot read.

I know it is not a hardware issue because when i switch this port to the debug instance it works correctly. Something must be configuring it differrently when used as Debug.

 

Please Help!!!

ラベル(1)
タグ(2)
0 件の賞賛
返信
3 返答(返信)

2,173件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hello Joseph,

please, where do you have any array for received characters?

Can you attach whole project?

Best Regards,

Iva

0 件の賞賛
返信

2,173件の閲覧回数
josephgundel
Contributor III

I cannot post the whole project > I am trying to just read one character at a time or call the ISR. It does not do either

0 件の賞賛
返信

2,173件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hello Joseph,

never mind, please just send me part of the code where you work with uart.

I mean pin settings on UART, UART settings, interrupts...

Thank you.

Iva

0 件の賞賛
返信