sprintf, PRINTF, DbgConsole_Printf with float and double

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

sprintf, PRINTF, DbgConsole_Printf with float and double

4,608 次查看
gerhardheinzel
Contributor I

I am using Kinetis Design Studio 3.2.0 with SDK 2.0 for the K64F development board.

After browsing a lot of confusing and conflicting information and some testing, I found the following concerning printf() with float and double values.

sprintf() comes from the newlib-nano, and in order to  activate floating point I need to set the following linker flag as described in many places:

printf2.png

The very useful debug console also has a PRINTF function, that maps to DbgConsole_Printf, which is implemented separately and independently. In order to activate its floating point option, one needs to define PRINTF_FLOAT_ENABLE:

printf1.png

The test program included below furthermore revealed a bug in the PRINTF=DbgConsole_Printf implementation:

The bit pattern 0xffffffff interpreted as a 32-bit signed integer should print as "-1" but wrongly prints as "1" instead.

Hope this helps some others to save time,

G

#include "fsl_debug_console.h"
#include "board.h"
#include "pin_mux.h"
#include "clock_config.h"
#include <math.h>
#include <stdio.h>

int main(void)
{
    uint8_t u8 = 0xffU;
    uint16_t u16 = 0xffffU;
    uint32_t u32 = 0xffffffffU;

    int8_t i8 = 100U;
    int16_t i16 = 20000U;
    int32_t i32 = 1000000000U;

    float f = sqrtf(2.0);
    double d = sqrt(2.0);
    char s[80];

    BOARD_InitPins();
    BOARD_BootClockRUN();
    BOARD_InitDebugConsole();

    PRINTF("\r\nprintf test\r\n\r\n");
    PRINTF("Using PRINTF = DbgConsole_Printf:\r\n\r\n");
    PRINTF("u8 = %u = %x\r\n", (unsigned int) u8, (unsigned int) u8);
    PRINTF("u16 = %u = %x\r\n", (unsigned int) u16, (unsigned int) u16);
    PRINTF("u32 = %u = %x\r\n", (unsigned int) u32, (unsigned int) u32);
    PRINTF("u8 as integer = %d\r\n", (int) u8);
    PRINTF("u16 as integer = %d\r\n", (int) u16);
    PRINTF("u32 as integer = %d\r\n", (int) u32);
    PRINTF("i8 = %d\r\n", (int) i8);
    PRINTF("i16 = %d\r\n", (int) i16);
    PRINTF("i32 = %d\r\n", (int) i32);
    PRINTF("negative i8 = %d\r\n", (int) -i8);
    PRINTF("negative i16 = %d\r\n", (int) -i16);
    PRINTF("negative i32 = %d\r\n", (int) -i32);
    PRINTF("float = %.16f\r\n", f);
    PRINTF("double = %.16f\r\n", d);

    PRINTF("\r\nUsing sprintf:\r\n\r\n");
    sprintf(s, "u8 = %u = %x\r\n", (unsigned int) u8, (unsigned int) u8);
    PRINTF("%s", s);
    sprintf(s, "u16 = %u = %x\r\n", (unsigned int) u16, (unsigned int) u16);
    PRINTF("%s", s);
    sprintf(s, "u32 = %u = %x\r\n", (unsigned int) u32, (unsigned int) u32);
    PRINTF("%s", s);
    sprintf(s, "u8 as integer = %d\r\n", (int) u8);
    PRINTF("%s", s);
    sprintf(s, "u16 as integer = %d\r\n", (int) u16);
    PRINTF("%s", s);
    sprintf(s, "u32 as integer = %d\r\n", (int) u32);
    PRINTF("%s", s);
    sprintf(s, "i8 = %d\r\n", (int) i8);
    PRINTF("%s", s);
    sprintf(s, "i16 = %d\r\n", (int) i16);
    PRINTF("%s", s);
    sprintf(s, "i32 = %d\r\n", (int) i32);
    PRINTF("%s", s);
    sprintf(s, "negative i8 = %d\r\n", (int) -i8);
    PRINTF("%s", s);
    sprintf(s, "negative i16 = %d\r\n", (int) -i16);
    PRINTF("%s", s);
    sprintf(s, "negative i32 = %d\r\n", (int) -i32);
    PRINTF("%s", s);
    sprintf(s, "float = %.16f\r\n", f);
    PRINTF("%s", s);
    sprintf(s, "double = %.16f\r\n", d);
    PRINTF("%s", s);

    while (1)
        ;
    return 0;
}

0 项奖励
回复
0 回复数