"Selected directory does not contain Kinetis SDK 2.x for KDS"

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

"Selected directory does not contain Kinetis SDK 2.x for KDS"

跳至解决方案
5,005 次查看
therealfreegeek
Contributor IV

From Kinetis SDK 2.x Project Wizaed, but it does, see pic below. I tried a couple of different folders and names, with the same result. Will try on another PC tomorrow.

 

Any thoughts?

135338_135338.jpgksdk 2.0.jpg

标签 (1)
1 解答
2,754 次查看
BlackNight
NXP Employee
NXP Employee

Hi Jim,

Looking at the XML file, it seems to me that you have selected 'gcc' and not Kinetis Design Studio for your package?

You have

  <tools>

    <tool id="armgcc" name="GCC ARM Embedded" version="4.9.2015.3" vendor="GCC ARM Embedded" vendor_url="http://launchpad.net/gcc-arm-embedded"/>

  </tools>

But it should be

  <tools>

    <tool id="kds" name="Kinetis Design Studio" version="3.0" vendor="NXP Semiconductors" vendor_url="http://www.nxp.com"/>

  </tools>

I suggest that you regenerate the package with KDS as toolchain on http://www.nxp/kex

pastedImage_0.png

I hope this helps,

Erich

在原帖中查看解决方案

8 回复数
2,754 次查看
sanketmeher
Contributor II

I am facing same issue

Is this issue solved ?

0 项奖励
回复
2,754 次查看
BlackNight
NXP Employee
NXP Employee

Have you checked the solution (that you have included KDS as toolchain to the SDK)?

I hope this helps,

Erich

2,754 次查看
BlackNight
NXP Employee
NXP Employee

The wizard reads that manifest file. Somehow it is not accepted by the wizard. Could you post that manifest file?

Erich

0 项奖励
回复
2,754 次查看
therealfreegeek
Contributor IV

Hi Erich,

Here is the file http://www.racediagnostics.com/home/uploads/images/jag/regulator/ksdk_manifest.xml

I tried it on another machine this morning with the same result.

Thanks

Jim

0 项奖励
回复
2,754 次查看
BlackNight
NXP Employee
NXP Employee

Hi Jim,

I confirm that this file does not work for me neither. I'm checking what could be wrong and report back.

Erich

2,755 次查看
BlackNight
NXP Employee
NXP Employee

Hi Jim,

Looking at the XML file, it seems to me that you have selected 'gcc' and not Kinetis Design Studio for your package?

You have

  <tools>

    <tool id="armgcc" name="GCC ARM Embedded" version="4.9.2015.3" vendor="GCC ARM Embedded" vendor_url="http://launchpad.net/gcc-arm-embedded"/>

  </tools>

But it should be

  <tools>

    <tool id="kds" name="Kinetis Design Studio" version="3.0" vendor="NXP Semiconductors" vendor_url="http://www.nxp.com"/>

  </tools>

I suggest that you regenerate the package with KDS as toolchain on http://www.nxp/kex

pastedImage_0.png

I hope this helps,

Erich

2,754 次查看
therealfreegeek
Contributor IV

Thanks for your patience.

0 项奖励
回复
2,754 次查看
Jmart
NXP Employee
NXP Employee

Welcome to SDK 2.0!

I tried to recreate the issue you've presented by following the steps below, but I was able to unable to recreate the issue and was able to select my K64 SDK 2.0 folder for a new project. Let me know if any of these steps help resolve your issue.

The following steps were a fresh installation of KDS 3.0 and a fresh build of SDK 2.0 for K64.

Downloaded: Kinetis Design Studio installer for Microsoft Windows 3.0.0 from http://www.nxp.com/kds (a few clicks from here)

Downloaded: Updates: Kinetis Design Studio for Kinetis 3.1.0 (Winows and Linux OS) from the same location as above

Downloaded: Service Pack: Eclipse add-on to add Kinetis SDK V2.x Project Wizard from the same location as above

1. Installed KDS 3.0

2. Unzipped the KDS 3.1.0 updates to a known location.

3. Installed the KDS 3.1.0 updates through the following steps.

Installation instructions

a. Run KDS 3.0.0

b. Select Window > Preferences

c. Select Install/Update > Available Software Sites

d. Add a new install site using the Add... button

e. Type name of the install site into the Name field (e.g. KDS 3.1.0).

f. Click on the Archive... button and find the KDS_3.1.0.zip.

g. Confirm site addition by clicking on OK button.

h. Close Preferences windows by clicking on OK button.

i. Select Help > Check for Updates

j. Continue with the wizard. Accept the license agreement during the installation process.

k. Restart KDS.

4. Installed the Kinetis SDK v2.x project wizard  through the following steps.

Installation Instructions

a. Start Kinetis Design Studio

b. Select the menu Help > Install New Software

c. Click 'Add' button and type Name = "New Kinetis SDK 2.x Project Wizard", Location = select: NPWforKinetisSDK2x.zip

d. Confirm installation

5. Login to http://kex.nxp.com and issue a build for K64 with KDS toolchain support. I did omit the inclusion of FreeRTOS for this test archive. I wouldn't see that as the root cause of your issue, but please let me know if that makes a difference.

6. Unzip the SDK 2.0 archive to a known location (C:\nxp) and start the new project Wizard for an SDK 2.x project

7. Enter a project name and select the folder in which you've placed your SDK 2.0 K64 archive.

Here's a screenshot of what I see when adding a new project. I was able to subsequently add all of the drivers and build the NPW project.

sdk_2.0.JPG

If these steps do not help you resolve the issue, please let me know which toolchain options you selected for your SDK build in Kex as this is the only variable that I can think of that may cause this issue.

Regards

0 项奖励
回复