problem using 2 i2c

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

problem using 2 i2c

1,493件の閲覧回数
hunglam
Contributor II

I use a custom board with the k64 as the mcu, kinetis design studio and ksdk1.2. on the board are 2 i2c devices connected to i2c_0 and i2c_1 of the k64. When I connect only one of the i2c devices in my program, no problem! but if I try to connect to both devices, i2c_1 cannot be connected?! why?

thanks in advance for any help

ラベル(1)
0 件の賞賛
返信
1 返信

1,372件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello hung Iam:

What do you mean with "cannot be connected"? What kind of behavior do you see?

Please explain more about your issue so we are able to help. For example:

Which I2C0 and I2C1 pins you use?

Is your application using any RTOS (e.g. MQX, FreeRTOS)?

Do you miss data or there is no signal in the bus?

And if possible post the relevant code or project so we can give it a check.

Regards!

Jorge Gonzalez

0 件の賞賛
返信