prasimax - KL82

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

prasimax - KL82

1,271 Views
ThingPiaoChew
NXP Employee
NXP Employee

One of my customer is using KL82 and have some enquries on the Boot loader of KL82 . 

Do we have utility tools (support Windows/Linux) for updating firmware through USB bootloader .??

 

0 Kudos
Reply
1 Reply

1,179 Views
Kan_Li
NXP TechSupport
NXP TechSupport

yes, we have such kind of tools available, after installing Kboot, you may find them in the following folder:

pastedImage_1.png

blhost supports linux , mac and windows, you may refer to the user guider in the doc folder for more details.

pastedImage_2.png


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply