ow i can to use the libraries of RTCESL with KSDK v2.0 in KDS v3 ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ow i can to use the libraries of RTCESL with KSDK v2.0 in KDS v3 ?

1,241 Views
saulogarcia
Contributor I

Hello Nxp community. i would like to know how i can to use the libraries of RTCESL with KSDK v2.0 in KDS v3 ?, i appreciate your help.

King Regards!!!

Labels (1)
0 Kudos
Reply
1 Reply

1,123 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Saulo,

Pls download the motor control library from the link:

For a library, you just need to integrate the library to the application project, include the protype *.h, it is okay. The library is not dependent on the SDK, but dependent on the tools for example, for IAR, KDS. Furthermore, because Cortex-M0/M4/M7 use different instruction set, the library is also dependent on core in other words, the sub-family of Kinetis.
BR
Xiangjun Rong
0 Kudos
Reply