mbed

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决
2,065 次查看
ericeckenrode
Contributor I


Hello,

we would like to use the K65F and 3.0 mbed.  However, today it looks like the KSDK ported is dated.

mbed-hal-ksdk-mcu/mbed-hal-ksdk-mcu/TARGET_KSDK_CODE/hal at master · ARMmbed/mbed-hal-ksdk-mcu · Git...

 

It looks like K65F is only partially supported in this version (certain drivers are missing.  Ex.. lpuart, high speed USB, sdram, etc...).

 

It is known when the latest version of KSDK will be ported into the mbed platform??

Also, is Freescale responsible for this port or does it default to mbed for the port?

 

Thanks in advance,
Eric

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,904 次查看
mnorman
NXP Employee
NXP Employee

Eric,

Freescale worked with ARM to enable the FRDM-K64F mbed support, but as you noted it is based on an older version of the KSDK. We do plan to update the support for K64F and add more Kinetis devices in early 2016 based on KSDK v1.3 and later.  The exact timing isn't known at this time. 

The best place to discuss ARM mbed support is probably on the ARM mbed community with the developers who are actively contributing. 

-Michael

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,905 次查看
mnorman
NXP Employee
NXP Employee

Eric,

Freescale worked with ARM to enable the FRDM-K64F mbed support, but as you noted it is based on an older version of the KSDK. We do plan to update the support for K64F and add more Kinetis devices in early 2016 based on KSDK v1.3 and later.  The exact timing isn't known at this time. 

The best place to discuss ARM mbed support is probably on the ARM mbed community with the developers who are actively contributing. 

-Michael

0 项奖励
回复
1,904 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

amh​ are you able to comment here?

0 项奖励
回复