k66f with gt202

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

k66f with gt202

1,603件の閲覧回数
srinivas
Contributor I

Any one is successful in interfacing  gt202 wifi module with k66f board??

0 件の賞賛
返信
1 返信

1,496件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Srinivas Ardha,

     We still don't have the direct K66 GT202 sample code, you can refer to FRDM-K64 SDK code, that have the according with GT202.

    BTW, the GT202 is EOL now, it's better to use the silex board:SX-ULPAN-2401-SHIELD.

Wish it helps you!

If you still have question about it, please kindly let me know.

Have a great day,
Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信