frdm-k22f hangs on board_clockinit with segger j-link debugger

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

frdm-k22f hangs on board_clockinit with segger j-link debugger

Jump to solution
1,987 Views
dkm
Contributor I

KDK 3.0.0

KSDK 1.2.0

FRDM-K22F

OpenSDA v 2.1

 

System hangs when calling CLOCK_SYS_SetConfiguration.

 

Tried adding jumper J21 per some discussion that this could be related to a VBat issue. No luck.

 

Thanks

Labels (1)
1 Solution
1,854 Views
dkm
Contributor I

Thanks for the offer of help...

It turns out it was caused by an chip selection error while following a Getting Started tutorial. I had mistakenly picked an MK24F processor instead of the MK22F51212 chip that is used on the FRDM-K22F evaluation board. Who would'a thunk!

Thanks again!

View solution in original post

2 Replies
1,854 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello D K,

Which Clock mode do you configure ?

Please show how to the configuration about the  function "CLOCK_SYS_SetConfiguration"

or send your project to me , i will test it no my side.

BR

Alice

0 Kudos
Reply
1,855 Views
dkm
Contributor I

Thanks for the offer of help...

It turns out it was caused by an chip selection error while following a Getting Started tutorial. I had mistakenly picked an MK24F processor instead of the MK22F51212 chip that is used on the FRDM-K22F evaluation board. Who would'a thunk!

Thanks again!