canCom2:fsl_flexcan Processor Expert Component will not generate Code

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

canCom2:fsl_flexcan Processor Expert Component will not generate Code

跳至解决方案
4,161 次查看
robertheldibrid
Contributor I

I am using a TWR-KV46F150M board.  I have Knietis SDK v.1.3.0_KV4xF_1.0.0 installed.  I would like to use the driver fsl_flexcan Peripheral Driver.  I added it to the Components, everything looks filled out.  I am not sure where the setup is done.  I am assuming the application will have to call some functions. 

 

The problem is when I try to generate the code, I get the following message

ERROR: Not possible to run: Drivers\Kinetis\printConfigs.js. javax.script.ScriptException: sun.org.mozilla.javascript.internal.EcmaError: TypeError: Cannot find function getEditorData in object com.processorexpert.core.service.api.internal.PExInspectorIntegerItemAPI@680703. (<Unknown source>#89) in <Unknown source> at line number 89

 

Any ideas what I am missing? 

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
4,060 次查看
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Robert Heldibridle

What version of IDE do you have? I'm using KDS 3.2 and processor expert 3.0.2 and I don't see this problem.

Capture.PNG

Also, what OS do you have?


Have a great day
Jorge Alcala

在原帖中查看解决方案

0 项奖励
回复
4 回复数
4,060 次查看
robertheldibrid
Contributor I

I upgraded Processor Expert and now it works.  I think I had version 3.0.0.  Thanks for your help.

0 项奖励
回复
4,060 次查看
robertheldibrid
Contributor I

Thanks for getting back to me,

This is from the help...

  KSDK 1.3.0 KV4xF Eclipse Update1.0.0.b151015com.freescale.processorexpert.kinetis-168mhz-kv4xf.sp.feature.groupFreescale Semiconductor, Inc.
    Processor Expert Kinetis SDK Support1.2.0.RT7_b1515-0427com.freescale.processorexpert.feature.core.kpsdk.feature.groupFreescale Semiconductor, Inc.
  Processor Expert for Kinetis3.0.0.RT7_b1515-0427com.freescale.processorexpert.kinetis.feature.feature.groupFreescale Semiconductor, Inc.
    Pin Settings1.1.0.RT7_b1515-0427com.freescale.processorexpert.feature.pinsettings.feature.groupFreescale Semiconductor, Inc.
    Processor Expert Base UI1.4.0.RT7_b1515-0427com.freescale.processorexpert.feature.core.ui.feature.groupFreescale Semiconductor, Inc.
    Processor Expert Base Wizards1.4.0.RT7_b1515-0427com.freescale.processorexpert.feature.core.wizards.feature.groupFreescale Semiconductor, Inc.
    Processor Expert Core1.4.0.RT7_b1515-0427com.freescale.processorexpert.feature.core.feature.groupFreescale Semiconductor, Inc.
    Processor Expert Custom Views1.0.0.RT7_b1515-0427com.freescale.processorexpert.feature.custom.mcu.feature.groupFreescale Semiconductor, Inc.
    Processor Expert Flexnet License1.0.0.RT7_b1515-0427com.freescale.processorexpert.feature.license.feature.groupFreescale Semiconductor, Inc.

I think I have everything. 

0 项奖励
回复
4,061 次查看
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Robert Heldibridle

What version of IDE do you have? I'm using KDS 3.2 and processor expert 3.0.2 and I don't see this problem.

Capture.PNG

Also, what OS do you have?


Have a great day
Jorge Alcala

0 项奖励
回复
4,060 次查看
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Robert Heldibridle

I'm working in your issue, Did you install the eclipse update for KSDK 1.3.0 KV4xF ? Could you please check the installation details and tell us if you can see KSDK 1.3.0 KV46xF Eclipse Update and processor Expert for kinetis?

I've created the project based on your description and I do not see any problem with code generation.


Have a great day,
Jorge Alcala

0 项奖励
回复