buffer overrun in KSDK_1.1, fsl_debug_console.c::debug_scanf()

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

buffer overrun in KSDK_1.1, fsl_debug_console.c::debug_scanf()

2,860 Views
björnhammarberg
Contributor II

As far as I can tell, there will be a buffer overrun if the user writes IO_MAXLINE number of characters due to the line

temp_buf[i + 1] = '\0';

Labels (1)
Tags (3)
0 Kudos
Reply
5 Replies

2,536 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi Bjorn,

I don't see the problem here. Could you explain?

Regards,

Carlos

0 Kudos
Reply

2,536 Views
björnhammarberg
Contributor II

Certainly. I have included the source for clarity.

The temp_buf buffer is IO_MAXLINE characters long [0..IO_MAXLINE-1].

The for loop allows characters to be entered from 0 to IO_MAXLINE-1.

If the input stream provides characters continuously and none of them is a newline '\n', the loop will eventually enter at i = IO_MAXLINE-1.

Following that, the erroneous line will be executed with this value of i.

This results in an end-of-string character '\0' being put at temp_buf[IO_MAXLINE] which is *outside* of the buffer!

This results in either the ap variable or some stack-stored registers (I am not sure of the "direction" of the buffer overrun) getting altered which, either way, can not be desirable.

Nonetheless, there is a (potential) buffer overrun and I think it should be removed.

All the best,

Björn

int debug_scanf(const char  *fmt_ptr, ...)

{

    char    temp_buf[IO_MAXLINE];

    va_list ap;

    uint32_t i;

    char result;

    va_start(ap, fmt_ptr);

    temp_buf[0] = '\0';

    for (i = 0; i < IO_MAXLINE; i++)

    {

        temp_buf[i] = result = debug_getchar();

        if (result == '\n')

        {

            /* End of Line */

            break;

        }

        temp_buf[i + 1] = '\0';

    }

  

    result = scan_prv(temp_buf, (char *)fmt_ptr, ap);

    va_end(ap);

   return result;

}

0 Kudos
Reply

2,536 Views
PatriciaTeran
Contributor III

Hi, Bjorn

I apologize for the late response, are you still having the same issue?

Regards

Patricia

0 Kudos
Reply

2,536 Views
björnhammarberg
Contributor II

Sorry for even later response.

What do you mean by "still"? As far as I understand, the code is in error until it is fixed. Have you fixed it?

0 Kudos
Reply

2,536 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi Bjorn,

This is solved in KSDK1.3.

Thanks for your comments.


Best regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply