about RW data segment in K64 Linker script file

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

about RW data segment in K64 Linker script file

2,422 Views
ninesun
Contributor II

Hello 

      I have question about .bss segment in file MK64FN1M0xxx12_flash.ld, The R/W memory data area was divided among m_data and m_data_2.  but these two segment is continuous. why not  not take it as whole segment? if it can be taken as union segment. Then all data are use such memory area. for example. the .bss segment in my program is too large, i had to assign the .bss segment to m_data_2. Then some memory of m_data are to be wasted. Is there any reason to divided into two separated segment?

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

2,229 Views
BlackNight
NXP Employee
NXP Employee

Hi nine,

The reason is that the Kinetis K series has two memory controllers, one for each segment. So indeed there are two RAM ranges/segments, even if they are close together. You might face a hard fault if you place a variable/object over that 0x2000'0000 boundary depending on how you access it. More details about this you can find in https://mcuoneclipse.com/2013/07/10/freertos-heap-with-segmented-kinetis-k-sram/  (make sure you check the discussion area).

So you *could* have the two areas in one piece, but you need to be careful about what you do with your memory allocation.

I hope this helps,

Erich

2,230 Views
ninesun
Contributor II

Ok I see .Thanks

0 Kudos
Reply