Writing flash memory with KL27Z256

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Writing flash memory with KL27Z256

Jump to solution
3,037 Views
paolocolombo
Contributor III

Hi, to all!

I have a problem with my card realized with KL27Z256 using flash memory for storing parameters. (KDS Mainline SDK 3.0.0 + 1.2.0)

I followed the demo attached to the package SDK 1.2.0 Mainline, made for KL24Z64.

For several days I'm working, but I managed to write and delete only addresses equal to or greater than 0x20000, in the second block of flash then.

I need to be able to use an address in the first 128K and here the problems begin, because in this case the processor reset continuously, and the write / erase are unsuccessful.

I note that, as indicated by the demo, I copied in the ram "CommandSequence" and the "CallBack" (which is empty).

I enclose lines of code involved and screen component inspector.

 

void
Store_Param(void)

{

              
StartFlashAddr = K_StartFlashAddr;                                     // 0x20000              
Size = K_SectorSize;                                                             // 0x0400        

               
flash1_InitConfig0.CallBack = (PCALLBACK)RelocateFunction((uint32_t)__ram_for_callback , CALLBACK_SIZE , (uint32_t)flash1_Callback);

MyCommandSequence  = (pFLASHCOMMANDSEQUENCE)RelocateFunction((uint32_t)__ram_func , LAUNCH_CMD_SIZE, (uint32_t)FlashCommandSequence);

               
          ret = FlashEraseSector(&flash1_InitConfig0, StartFlashAddr, Size, MyCommandSequence);

               
          ParamSet.Cks = Calc_CKS((byte *)&ParamSet, sizeof(ParamSet) - 1);

              
          Size = sizeof(ParamSet);

          ret = FlashProgram(&flash1_InitConfig0, StartFlashAddr, Size, (byte*)&ParamSet, MyCommandSequence);

          f_To_Save = FALSE;

 

}             // Store_Param

 



39411_39411.pngpastedImage_0.png

Labels (1)
Tags (1)
1 Solution
2,404 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Paolo Colombo:

In your configuration the Program Flash size is incorrect, it should be 0x00040000 instead of 0xFFFFFFFF.

To resolve the reset problem, try enabling the ESFC bit as instructed by colleague Jennie Zhang in her document:

Using ESFC bit - Flash programming routines in Cotex M0+ kinetis MCU

Just add this line of code:

MCM_PLACR |= MCM_PLACR_ESFC_MASK;

Refer to the attached code for an example, which erases and writes data to the last sector in block 0.

Let me know if the problem persists.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
2,405 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Paolo Colombo:

In your configuration the Program Flash size is incorrect, it should be 0x00040000 instead of 0xFFFFFFFF.

To resolve the reset problem, try enabling the ESFC bit as instructed by colleague Jennie Zhang in her document:

Using ESFC bit - Flash programming routines in Cotex M0+ kinetis MCU

Just add this line of code:

MCM_PLACR |= MCM_PLACR_ESFC_MASK;

Refer to the attached code for an example, which erases and writes data to the last sector in block 0.

Let me know if the problem persists.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,404 Views
paolocolombo
Contributor III

Congratulations !!! I solved this problem immediately !!!

The problem was right:

MCM_PLACR |= MCM_PLACR_ESFC_MASK;

Thank you very much, you are a magician!