Why cant i change CAN bus bit rate to 500kbps on MK20?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why cant i change CAN bus bit rate to 500kbps on MK20?

1,661 Views
yarannan
Contributor III

Hi there,

I am using KSDK1.2 on KDS 3.0 with MK20DX256VL10.

I tried to follow the K60 CAN example. And so far, two

of can bit rate configuration (125kbps and 250 kbps) works.

Once i move up to 500kbps. It doesnt work anymore.

The physical interface I used is NXP TJA1051. It could go

up to 2Mbits/s.

 

Is there any thing that I probably missed from above?

Please point out. I am really frustrated...

 

Thanks,

 

Yaran

Labels (1)
Tags (4)
0 Kudos
Reply
1 Reply

1,285 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Please refer below FlexCAN bit timing setting for 500KHz, which is based on TWR-K60D100M with bus clock 48MHz:

2015-12-11_14-58-01.png

Wish it helps.
Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply