Why Kinetis SDK doesn't support the MK60DN512Z?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why Kinetis SDK doesn't support the MK60DN512Z?

1,263 Views
sergeyzubov
Contributor I

Helloo! I have tried to configure a "Hello, world" example on KSDK with MK60DN512 but it doesn't work with Z processor.

 

With best regards, Serg

Labels (1)
0 Kudos
Reply
2 Replies

1,073 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Sergey Zubov:

The parts with Z are from an old revision of silicon. The differences between such parts and the latest revisions are detailed in the application note AN4445.

The old revision is not recommended for new designs and so it will not be supported with KSDK.

You can get new parts or you can still use you available chips with Processor Expert drivers.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,073 Views
sergeyzubov
Contributor I

Hello, Jorge!

Thank you very match!

I will use new version.

With best regards, Sergey Zubov

0 Kudos
Reply