Where I can get the SDK for Kinetis? All the download links to it are broken, including the MCUXpresso SDK.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Where I can get the SDK for Kinetis? All the download links to it are broken, including the MCUXpresso SDK.

2,363 次查看
eugeniomanrique
Contributor I

The MCUXpresso SDK is supposed to replace Kinetis SDK, but the link to download is not working.

标记 (1)
0 项奖励
回复
3 回复数

2,209 次查看
BlackNight
NXP Employee
NXP Employee

Welcome to MCUXpresso | MCUXpresso Config Tools  is working for me. As well the link to the builder for the SDK:

https://mcuxpresso.nxp.com/en/builder 

I hope this helps,

Erich

0 项奖励
回复

2,208 次查看
eugeniomanrique
Contributor I

Hi Erich,

The download is not working yet, after asking for it gives a Page Not Found:

Any idea why is this happening ?

Eugenio Manrique Forseck

emf54@icloud.com

El 05/03/2017, a las 1:05 p.m., BlackNight <admin@community.nxp.com> escribió:

NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: Where I can get the SDK for Kinetis? All the download links to it are broken, including the MCUXpresso SDK.

reply from Erich Styger <https://community.nxp.com/people/BlackNight?et=watches.email.thread> in Kinetis Software Development Kit - View the full discussion <https://community.nxp.com/message/883683?commentID=883683&et=watches.email.thread#comment-883683>

Welcome to MCUXpresso | MCUXpresso Config Tools <https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fmcuxpresso.nxp.com%2Fen%2Fwelcome> is working for me. As well the link to the builder for the SDK:

https://mcuxpresso.nxp.com/en/builder <https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fmcuxpresso.nxp.com%2Fen%2Fbuilder>

I hope this helps,

Erich

Reply to this message by replying to this email, or go to the message on NXP Community <https://community.nxp.com/message/883683?commentID=883683&et=watches.email.thread#comment-883683>

Start a new discussion in Kinetis Software Development Kit by email <mailto:discussions-community-kinetis-kinetissoftwaredevelopment--kit@mail.freescale.jiveon.com> or at NXP Community <https://community.nxp.com/choose-container.jspa?contentType=1&containerType=14&container=11234&et=watches.email.thread>

Following Re: Where I can get the SDK for Kinetis?  All the download links to it are broken, including the MCUXpresso SDK. <https://community.nxp.com/message/883683?commentID=883683&et=watches.email.thread#comment-883683> in these streams: Inbox

This email was sent by NXP Community because you are a registered user.

You may unsubscribe <https://community.nxp.com/unsubscribe.jspa?email=emf54%40icloud.com&token=0c7163dc06bd0a77b6132e7378894f33fa4555968087b101d126c00e3d3650b1> instantly from NXP Community, or adjust email frequency in your email preferences <https://community.nxp.com/user-preferences!input.jspa>

0 项奖励
回复

2,208 次查看
BlackNight
NXP Employee
NXP Employee

Hi Eugenio,

I think it is a problem with your ISP, because it works for me?

pastedImage_1.png

Erich

0 项奖励
回复