What is the difference between Kinetis SDK mainline & standalone?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the difference between Kinetis SDK mainline & standalone?

1,806 Views
Kenm
Contributor II

What is the difference between Kinetis SDK mainline & standalone versions?

Labels (1)
0 Kudos
Reply
1 Reply

1,298 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Ken Maitland:

The KSDK mainline includes support for a range of Kinetis MCU families excepting those of the Standalone versions.

The KSDK standalone versions are packages released after the mainline version targeted for a specific Kinetis development board or Kinetis family, whose support for some reason did not make it to the release of the mainline version (e.g. time constraints, hardware not ready yet or tests not completed).

All of the standalone packages are based on a specific KSDK version such as the mainline packages, so all of the software layers are compatible with that version (drivers, HAL, stacks, etc.).

I hope this helps clarifying.

Regards!

Jorge Gonzalez

0 Kudos
Reply