Using USB CDC device with Windows CE Host

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using USB CDC device with Windows CE Host

1,586件の閲覧回数
jesperpape
Contributor II

Hello,

 

Can anyone confirm whether the KSDK 1.3.0 USB device stack has been tested against a Windows CE Host?

We are running the the TWRK65F180M USB CDC device demo (C:\Freescale\KSDK_1.3.0\examples\twrk65f180m\demo_apps\usb\device\cdc\virtual_com) and we can connect to a laptop with out problems. But we are struggling to get a Windows CE host to recognize the USB device.

 

Anyone having experience with this?

 

 

Best regards

Jesper Larsen

ラベル(1)
タグ(2)
1 返信

1,435件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hi Jesper,

Until now we have not tested the device CDC example with any Windows CE Host.

But the device CDC example is guaranteed to work under Windows XP/7/8/10, Linux (like Ubuntu), ANdroid(like our i.MX) and MAC OS.

Have a nice day.

Iva