Using FTM_SetupInputCapture

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Using FTM_SetupInputCapture

跳至解决方案
2,909 次查看
henninjw
Contributor II

Hi Everyone,

Im new to using Kinetis microcontrollers and I have a TWR-K65F180M board that I'm trying to use to capture inputs from an encoder.  I am working off of the PWM_twochannel driver example using SDK2.0. I have the FTM set up to use FTM2_CH0.  The api document says that every time a rising edge is captured the counter value should be stored in the CnV register.  However, unable to read any values in the CnV registers using the EmbSysRegView.

 

Thanks for any help!

 

145529_145529.pngpastedImage_2.png145530_145530.pngpastedImage_3.png145531_145531.pngpastedImage_4.png

标签 (1)
0 项奖励
回复
1 解答
2,515 次查看
isaacavila
NXP Employee
NXP Employee

Hello Jake,

Just as reference, here is the full example:

/*******************************************************************************

* Definitions

******************************************************************************/

#define BOARD_FTM_BASEADDR          FTM2

#define BOARD_FIRST_FTM_CHANNEL     0U

#define BOARD_SECOND_FTM_CHANNEL    1U

/* Get source clock for FTM driver */

#define FTM_SOURCE_CLOCK            CLOCK_GetFreq(kCLOCK_BusClk)

#define FTM_READ_INPUT_CAPTURE  BOARD_FTM_BASEADDR->CONTROLS[BOARD_FIRST_FTM_CHANNEL].CnV

/*******************************************************************************

* Prototypes

******************************************************************************/

/*******************************************************************************

* Variables

******************************************************************************/

/*******************************************************************************

* Code

******************************************************************************/

/*!

* @brief Main function

*/

int main(void)

{

    ftm_config_t ftmInfo;

    uint32_t status = 0;

    /* Board pin, clock, debug console init */

    BOARD_InitPins();

    BOARD_BootClockRUN();

    BOARD_InitDebugConsole();

    /* Print a note to terminal */

    PRINTF("\r\nFTM input capture example\r\n");

    FTM_GetDefaultConfig(&ftmInfo);

    /* Initialize FTM module */

    FTM_Init(BOARD_FTM_BASEADDR, &ftmInfo);

    PRINTF("FTM value: \r\n");

    FTM_SetupInputCapture(BOARD_FTM_BASEADDR, BOARD_FIRST_FTM_CHANNEL, kFTM_RisingEdge, 0);

    BOARD_FTM_BASEADDR->MOD = 0xFFFF;

    FTM_StartTimer(BOARD_FTM_BASEADDR, kFTM_SystemClock);

    while (1)

    {

        if (FTM_READ_INPUT_CAPTURE >= 20000) {

            PRINTF("%d\r\n",FTM_READ_INPUT_CAPTURE);

        }

        status = FTM_GetStatusFlags(BOARD_FTM_BASEADDR);

        if (status & kFTM_TimeOverflowFlag) {

            FTM_ClearStatusFlags(BOARD_FTM_BASEADDR, status);

        }

    }

}

Hope this helps!

Regards,

Isaac

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,515 次查看
isaacavila
NXP Employee
NXP Employee

Hello Jake,

Sorry for late response. For input capture mode, you will need to set 0xFFFF to MOD register in order to use counter in free-running mode. Program should look like as follows:

#define FTM_READ_INPUT_CAPTURE  BOARD_FTM_BASEADDR->CONTROLS[BOARD_FIRST_FTM_CHANNEL].CnV

 

    ftm_config_t ftmInfo;

    uint32_t status = 0;

    /* Board pin, clock, debug console init */

    BOARD_InitPins();

    BOARD_BootClockRUN();

    BOARD_InitDebugConsole();

    /* Print a note to terminal */

    PRINTF("\r\nFTM input capture example\r\n");

    FTM_GetDefaultConfig(&ftmInfo);

    /* Initialize FTM module */

    FTM_Init(BOARD_FTM_BASEADDR, &ftmInfo);

    PRINTF("FTM value: \r\n");

    FTM_SetupInputCapture(BOARD_FTM_BASEADDR, BOARD_FIRST_FTM_CHANNEL, kFTM_RisingEdge, 0);

    BOARD_FTM_BASEADDR->MOD = 0xFFFF;

    FTM_StartTimer(BOARD_FTM_BASEADDR, kFTM_SystemClock);

    while (1)

    {

        if (FTM_READ_INPUT_CAPTURE >= 20000) {

            PRINTF("%d\r\n",FTM_READ_INPUT_CAPTURE);

        }

        status = FTM_GetStatusFlags(BOARD_FTM_BASEADDR);

        if (status & kFTM_TimeOverflowFlag) {

            FTM_ClearStatusFlags(BOARD_FTM_BASEADDR, status);

        }

    }

If you try this code, you will be able to print on screen counter value.

I hope this can help you!

Regards,

Isaac

0 项奖励
回复
2,515 次查看
henninjw
Contributor II

Isaac,

Thanks for the help.  I am still having some issues with the BOARD_FIRST_FTM_CHANNEL. Just to clarify I need to define BOARD_FIRST_FTM_CHANNEL as kFTM_Chnl_0 and BOARD_FTM_BASEADDR as FTM2 to capture input from FTM2_CH0 that will measure the time between riding edges and print this to the screen.

Thanks again

0 项奖励
回复
2,515 次查看
isaacavila
NXP Employee
NXP Employee

Hello Jake,

Just as reference, here is the full example:

/*******************************************************************************

* Definitions

******************************************************************************/

#define BOARD_FTM_BASEADDR          FTM2

#define BOARD_FIRST_FTM_CHANNEL     0U

#define BOARD_SECOND_FTM_CHANNEL    1U

/* Get source clock for FTM driver */

#define FTM_SOURCE_CLOCK            CLOCK_GetFreq(kCLOCK_BusClk)

#define FTM_READ_INPUT_CAPTURE  BOARD_FTM_BASEADDR->CONTROLS[BOARD_FIRST_FTM_CHANNEL].CnV

/*******************************************************************************

* Prototypes

******************************************************************************/

/*******************************************************************************

* Variables

******************************************************************************/

/*******************************************************************************

* Code

******************************************************************************/

/*!

* @brief Main function

*/

int main(void)

{

    ftm_config_t ftmInfo;

    uint32_t status = 0;

    /* Board pin, clock, debug console init */

    BOARD_InitPins();

    BOARD_BootClockRUN();

    BOARD_InitDebugConsole();

    /* Print a note to terminal */

    PRINTF("\r\nFTM input capture example\r\n");

    FTM_GetDefaultConfig(&ftmInfo);

    /* Initialize FTM module */

    FTM_Init(BOARD_FTM_BASEADDR, &ftmInfo);

    PRINTF("FTM value: \r\n");

    FTM_SetupInputCapture(BOARD_FTM_BASEADDR, BOARD_FIRST_FTM_CHANNEL, kFTM_RisingEdge, 0);

    BOARD_FTM_BASEADDR->MOD = 0xFFFF;

    FTM_StartTimer(BOARD_FTM_BASEADDR, kFTM_SystemClock);

    while (1)

    {

        if (FTM_READ_INPUT_CAPTURE >= 20000) {

            PRINTF("%d\r\n",FTM_READ_INPUT_CAPTURE);

        }

        status = FTM_GetStatusFlags(BOARD_FTM_BASEADDR);

        if (status & kFTM_TimeOverflowFlag) {

            FTM_ClearStatusFlags(BOARD_FTM_BASEADDR, status);

        }

    }

}

Hope this helps!

Regards,

Isaac

0 项奖励
回复