Update fails for New Kinetis SDK 2.x Project Wizard

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Update fails for New Kinetis SDK 2.x Project Wizard

3,587 Views
JimDon
Senior Contributor III

And other updates that I installed manually.

An error occurred while collecting items to be installed

session context was:(profile=DefaultProfile, phase=org.eclipse.equinox.internal.p2.engine.phases.Collect, operand=, action=).

Artifact not found: http://freescale.com/lgfiles/updates/Eclipse/KDS/features/com.nxp.feature.npw4sdk_1.0.1.201603011011....

http://freescale.com/lgfiles/updates/Eclipse/KDS/features/com.nxp.feature.npw4sdk_1.0.1.201603011011...

 

Also:

An error occurred while collecting items to be installed

session context was:(profile=DefaultProfile, phase=org.eclipse.equinox.internal.p2.engine.phases.Collect, operand=, action=).

Artifact not found: http://freescale.com/lgfiles/updates/Eclipse/KDS/features/com.freescale.projectofprojects.eclipse_1.....

http://freescale.com/lgfiles/updates/Eclipse/KDS/features/com.freescale.projectofprojects.eclipse_1....

None of the updates from fsl kds - http://freescale.com/lgfiles/updates/Eclipse/KDS

seem to work.

Labels (1)
Tags (1)
5 Replies

3,324 Views
ivadorazinova
NXP Employee
NXP Employee

Hi Jim,

thank you for your feedback.

We know about the issue and actually work on it.

I will let you know when issue will be fixed.

Best Regards,

Iva

0 Kudos
Reply

3,325 Views
JimDon
Senior Contributor III

Any chance we can get URLS for the jars so we can manually install them?

Thanks,

Jim

0 Kudos
Reply

3,324 Views
ivadorazinova
NXP Employee
NXP Employee

Hi Jim,

now it works. There was a mistake on our site.

Please, can you confirm it on your side?

ProjectWizard.png

Thank you.

Have a nice day.

Iva

0 Kudos
Reply

3,325 Views
JimDon
Senior Contributor III

Yes that is what I see, but it is saying that it is already installed ??? The next button does not light up, but it says on the list?

I have check hide item already installed, but it still shows them???

0 Kudos
Reply

3,324 Views
ivadorazinova
NXP Employee
NXP Employee

Hi Jim,

yes, because I tested it on my side and after that I post the result.

Best Regards,

Iva

0 Kudos
Reply