USBDM 4.6.10.250a Install problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USBDM 4.6.10.250a Install problem

1,740 Views
GeorgeChamberla
Contributor I

I have installed:-

USBDM_4_10_6_250a_Win  and  USBDM_Drivers_1_3_0_Win_x64  on Windows 7

 

Using 'ARM GDB Server' setup I can detect the MKE04Z804 processor OK  on my FRDM-KE04Z Dev PCB

 

But I get the following error on exit:-

Welcome to USBDM GDB server

ERROR: Could not create server at the specified port !

 

Please Help

Labels (1)
0 Kudos
Reply
2 Replies

1,546 Views
pgo
Senior Contributor V

Hi George,

The only time I have seen this error is when there is already a program using that port.

I assume you are experimenting with the stand-alone server launched from the Windows Start Menu.  Can you try changing the server port if you have not already tried this.

pastedImage_0.png

The only other suggestion is related to networking and firewalls.  Is it possible that the GDB server is not allowed to create sockets?

bye

0 Kudos
Reply

1,546 Views
GeorgeChamberla
Contributor I

Thanks for the reply.

Changing the GDB Server Port number fixed it.  Thank you.

0 Kudos
Reply