USBDM 4.6.10.250a Install problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

USBDM 4.6.10.250a Install problem

1,794 次查看
GeorgeChamberla
Contributor I

I have installed:-

USBDM_4_10_6_250a_Win  and  USBDM_Drivers_1_3_0_Win_x64  on Windows 7

 

Using 'ARM GDB Server' setup I can detect the MKE04Z804 processor OK  on my FRDM-KE04Z Dev PCB

 

But I get the following error on exit:-

Welcome to USBDM GDB server

ERROR: Could not create server at the specified port !

 

Please Help

标签 (1)
0 项奖励
回复
2 回复数

1,600 次查看
pgo
Senior Contributor V

Hi George,

The only time I have seen this error is when there is already a program using that port.

I assume you are experimenting with the stand-alone server launched from the Windows Start Menu.  Can you try changing the server port if you have not already tried this.

pastedImage_0.png

The only other suggestion is related to networking and firewalls.  Is it possible that the GDB server is not allowed to create sockets?

bye

0 项奖励
回复

1,600 次查看
GeorgeChamberla
Contributor I

Thanks for the reply.

Changing the GDB Server Port number fixed it.  Thank you.

0 项奖励
回复