USB High Speed on FRDM-K22F (KDS 1.0.0)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

USB High Speed on FRDM-K22F (KDS 1.0.0)

跳至解决方案
2,530 次查看
mohamedessadoun
Contributor I

Hi all,

I'm using FRDM-K22F board for a USB device application using KDS SDK.
I started from MSC sample to have bulk in/out.

All working fine except it is USB Full Speed.

I want to enable my device as HIGH_SPEED, I need to rebuild usbd_sdk_frdmk22f120m_mqx which needs EHCI as host controller interface.

The problem is, I cannot find the ehci interface source code anywhere in my KDSK while I have all concerning KHCI in "MQX_KSDK_1.0.0\usb\usb_core\device\sources\controller"


Am I missing something?

How to enable HIGH Speed config on K22F using KDS.

Thanks for your help.

标签 (1)
0 项奖励
回复
1 解答
2,274 次查看
mjbcswitzerland
Specialist V

Hi

The K22 has only FS USB.

For HS USB you will need something like a K70, plus external HW to interface its EHCI to the bus.

Regards

Mark

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,273 次查看
mohamedessadoun
Contributor I

Hi,

Was confusing between Kinetis platforms.

Anyway, having HS on this platform would have been great.

I will consider using K70.

Thanks for your time!

Regards.

0 项奖励
回复
2,275 次查看
mjbcswitzerland
Specialist V

Hi

The K22 has only FS USB.

For HS USB you will need something like a K70, plus external HW to interface its EHCI to the bus.

Regards

Mark

0 项奖励
回复
2,273 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Yes, and so far, KSDK hasn't support EHCI yet, just MQX and USB stack ver 4.1.1 supports EHCI driver, and customer may use TWR-K70F120M and TWR-SER2 together to run the EHCI demos. Now our team is adding EHCI support in KSDK, and you will have it in the future.


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------