Typo on Kinetis SDK v.2.1 API Reference Manual, for UART Send/receive using an interrupt method

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Typo on Kinetis SDK v.2.1 API Reference Manual, for UART Send/receive using an interrupt method

1,376 Views
phantomgz
Contributor IV

When I read "Kinetis SDK v.2.1 API Reference Manual", as the read box in below, is should be "UART1"

174843_174843.pngpastedImage_2.png

Cai.

Labels (1)
0 Kudos
Reply
1 Reply

1,241 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, ChaoXi,

Thank you for pointing out the typo, I will notify the DOC team of modifying it.

The correct prototype of the function is:

status_t UART_TransferSendNonBlocking (UART_Type  base, uart_handle_t  handle, uart_-
transfer_t  xfer)

BR

XiangJun Rong

0 Kudos
Reply