Touch Slider - FRDM KL25Z - SDK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Touch Slider - FRDM KL25Z - SDK

1,951 Views
mjc
Contributor I

Hello. I am trying to use the capacitive touch slider on FRDM-KL25Z. Does anyone have any example or tip to use it with Processor Expert (SDK 1.2.0), because when I add the TSS component the KDS show me this error: "The component is not supported for selected processor".149383_149383.JPGCapturar.JPG

Labels (1)
0 Kudos
Reply
2 Replies

1,519 Views
BlackNight
NXP Employee
NXP Employee

Hi Murilo,

that component indeed does not support the Kinetis SDK. If you want to use it, then you need to create/use a project without the Kinetis SDK.

Erich

0 Kudos
Reply

1,519 Views
mjc
Contributor I

Thanks!!!

0 Kudos
Reply