TWR-K70F120M kit - does the demo use the TSI (Touch Sense Input) module, or is it running custom code for touch sense? I can't find the project on the website, so I can't check the code myself.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TWR-K70F120M kit - does the demo use the TSI (Touch Sense Input) module, or is it running custom code for touch sense? I can't find the project on the website, so I can't check the code myself.

1,259 Views
arthurroberts
Contributor I

I've experienced some buggy behavior using the TWR-K70 touch sense buttons. I'd like to confirm that the kit is actually running the nxp TSI module code, or if it is custom. THe quick start guide says "download the demonstration labs at freescale.com/TWR-K70F120M", but of course there are no such labs there (AFAIK). Thanks!

Labels (1)
0 Kudos
Reply
1 Reply

1,116 Views
ivadorazinova
NXP Employee
NXP Employee

Hi Arthur,

Please go to TWR-K70F120M|Tower System Board|Kinetis MCUs|NXP and download demonstration labs here

Kinetis 120MHz bare metal sample code

there are some sample codes, for example TSI demo lowpower which is located under

<KINETIS_120MHZ_SC\KINETIS_120MHZ_SC_path>\build\<iar/cw>\TSI_demo_lowpower

I hope this helps you.

Best Regards,

Iva

0 Kudos
Reply