TWR-K70F120M kit - does the demo use the TSI (Touch Sense Input) module, or is it running custom code for touch sense? I can't find the project on the website, so I can't check the code myself.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

TWR-K70F120M kit - does the demo use the TSI (Touch Sense Input) module, or is it running custom code for touch sense? I can't find the project on the website, so I can't check the code myself.

882 次查看
arthurroberts
Contributor I

I've experienced some buggy behavior using the TWR-K70 touch sense buttons. I'd like to confirm that the kit is actually running the nxp TSI module code, or if it is custom. THe quick start guide says "download the demonstration labs at freescale.com/TWR-K70F120M", but of course there are no such labs there (AFAIK). Thanks!

标签 (1)
0 项奖励
回复
1 回复

739 次查看
ivadorazinova
NXP Employee
NXP Employee

Hi Arthur,

Please go to TWR-K70F120M|Tower System Board|Kinetis MCUs|NXP and download demonstration labs here

Kinetis 120MHz bare metal sample code

there are some sample codes, for example TSI demo lowpower which is located under

<KINETIS_120MHZ_SC\KINETIS_120MHZ_SC_path>\build\<iar/cw>\TSI_demo_lowpower

I hope this helps you.

Best Regards,

Iva

0 项奖励
回复