Sending of packets of udp of times a second.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Sending of packets of udp of times a second.

1,562 Views
profprogrammer
Contributor III

Hi.

I used KSD + PE and lwip stack. controller MK60DN512 .

I  want send udp packets from 192.168.70.110 ip  to 192.168.70.111 ip.

  /* Write your local variable definition here */   struct netif fsl_netif0;   struct netif *ner;   ip_addr_t fsl_netif0_ipaddr, fsl_netif0_netmask, fsl_netif0_gw;   int err;      lwip_init();      IP4_ADDR(&fsl_netif0_ipaddr, 192,168,70,110);    IP4_ADDR(&fsl_netif0_netmask, 255,255,255,0);    IP4_ADDR(&fsl_netif0_gw, 192,168,70,1);    ner = netif_add(&fsl_netif0, &fsl_netif0_ipaddr, &fsl_netif0_netmask, &fsl_netif0_gw, NULL, ethernetif_init, ethernet_input);    if ( ner == NULL ) err++;    netif_set_default(&fsl_netif0);    netif_set_up(&fsl_netif0);      {        struct udp_pcb * pcb;        ip_addr_t ipaddr;        struct pbuf *p;        err_t err;        uint32_t dt = 0;        // get new pcb        dt |= ENET->EIR >> 27;          pcb = udp_new();        if (pcb == NULL) {            LWIP_DEBUGF(UDP_DEBUG, ("udp_new failed!\n"));            return;        }          // bind to any IP address on port 7        if (udp_bind(pcb, IP_ADDR_ANY, 9000) != ERR_OK) {            LWIP_DEBUGF(UDP_DEBUG, ("udp_bind failed!\n"));            return;        }        dt |= ENET->EIR >> 27;          p = pbuf_alloc (PBUF_TRANSPORT, 8, PBUF_RAM);            while (1){         OSA_TimeDelay(1000);         IP4_ADDR(&ipaddr, 192,168,70,111);             err = udp_sendto(pcb, p, &ipaddr, 9000);        }         // set udp_echo_recv() as callback function       // for received packets          //   udp_recv(pcb, udp_echo_recv, NULL);    }

 

This code doesn't send packets.

Prompt in what an error?

Labels (1)
0 Kudos
Reply
1 Reply

956 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi Prof,

have you seen this example? If not please take a look, you will find it useful.

C:\Freescale\KSDK_1.2.0\examples\<board>\demo_apps\lwip\lwip_udpecho_demo

Regards,

Carlos

0 Kudos
Reply