SPI doesn't work using KSDK 2.0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SPI doesn't work using KSDK 2.0

969 次查看
nestorgalera
Contributor I

Hello everyone, I would ask you if you have the same problem I have. I use MKL26Z256xxx4

 

First of all, I've tryed to run SPI communication using registers configuration. This is my favourite way but... I notice that when I enter data in SPI Data Register low (SPIx_DL), nothing works... What is going wrong? I do all the steps.. I think... Do you have any code using registers?

 

And as I saw that.. I tryed to use SPI with KSDK 2.0 functions.. For example "interrupt". But also doesn't work. I don't know what I'm doing wrong :S :S :S

 

Do you have any example... SIMPLE example PLEASE?, with no dependences to functions that call functions... Just one transfer from master to slave. That's all.

 

Thank you very much!

标签 (1)
标记 (2)
0 项奖励
回复
0 回复数