SPI doesn't work using KSDK 2.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPI doesn't work using KSDK 2.0

951件の閲覧回数
nestorgalera
Contributor I

Hello everyone, I would ask you if you have the same problem I have. I use MKL26Z256xxx4

 

First of all, I've tryed to run SPI communication using registers configuration. This is my favourite way but... I notice that when I enter data in SPI Data Register low (SPIx_DL), nothing works... What is going wrong? I do all the steps.. I think... Do you have any code using registers?

 

And as I saw that.. I tryed to use SPI with KSDK 2.0 functions.. For example "interrupt". But also doesn't work. I don't know what I'm doing wrong :S :S :S

 

Do you have any example... SIMPLE example PLEASE?, with no dependences to functions that call functions... Just one transfer from master to slave. That's all.

 

Thank you very much!

ラベル(1)
タグ(2)
0 件の賞賛
返信
0 返答(返信)