SPI Master and Slave

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPI Master and Slave

1,342件の閲覧回数
kiansengkoh
Contributor I

I am using two MK64FN and KDS 3.2 with KSDK 1.3. I want to implement SPI master and slave. I use ProcessExpert to add component 'DPSI' and configure Master and Slave configurations. The slave no reply (using DSPI_DRV_SlaveTransferBlocking (as I can see the Master signal on scope) and also the Events.c (SPI_1_IRQHandler) seems not working. Connection: SPI0-SPI1, SIN-SOUT, SOUT-SIN, CLK-CLK-, CS-CS. 

0 件の賞賛
返信
1 返信

1,199件の閲覧回数
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Kian Seng Koh

Could you explain more your settings, it is complicate to follow what the problem could be.

For Processor Expert projects we recommend to check the propierities  of the component that is been used, you can right click in the component and go to "help on component". You can also check the examples of KSDK 1.3 for the dspi driver and see if you can run the code without problems.


Hope this information helps you
Have a great day,
Jorge Alcala

0 件の賞賛
返信