SGI with multiprocessing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SGI with multiprocessing

937 Views
khaledali
Contributor III


Hello all
I'm trying to run the test code generated in side the SDK multicore_test , it based on a Software Generated Interrupt  concept by changing the .
my problem is that the code itself doesn't work properly as only the software interrupt can be targeted from cpu 1 to
cpu 0 only
I also tried to generate the first interrupt by cpu2 and target it to CPU1 , the cpu1 also didn't serve the interrupt


to sum up what i really wants to do :
I need for proper steps for generating a Software interrupt from core0 targeting core1 and core1 handle the request.

Labels (1)
0 Kudos
Reply
0 Replies