SDRAM (16-bit) & FlexBus KSDK 2.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SDRAM (16-bit) & FlexBus KSDK 2.0

2,430件の閲覧回数
jankedzierski
Contributor II

Hello Everyone!

 

Can someone provide an example with KSDK 2.0 driver how to read/write to SDRAM connected to the FlexBus in such way (in att.)?

KSDK: 2.0

CPU: Kinetis MK26FN2M0VMI18

SDRAM: MT48LC8M16A2B4

(16-bits width, 4 banks, 4096 row, 512 cols)

Thank you.

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,243件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Jan,

Pls download SDK2.0 from the website:

Software Development Kit for Kinetis MCUs|NXP 

After you download the SDK2.0 based on MK26FN2M0xxx18, you can find out the directory:

C:\Freescale\SDK2.0_K26\boards\twrk65f180m\driver_examples\sdramc\kds

You can change the parameters based on your SDRAM chip.

Hope it can help you

BR

XiangJun Rong

0 件の賞賛
返信

2,243件の閲覧回数
jankedzierski
Contributor II

Oh yes. I've already got this example. But it is for 32-bit, ALE latch,... 

Has anyone example for TWR-K80? There is the same connection (almost same SDRAM)?

0 件の賞賛
返信