I'm trying to configure ethernet pins and gpio pin on PORTA. Any of the PORT_SetPinMux(PORTA, ..) calls will generate Hard Fault ( see code below). Any idea why it's happening?
PORT_SetPinMux(PORTA, PIN6_IDX, kPORT_MuxAsGpio); /* PORTA6 (pin 58) is configured as PTA6 */
PORT_SetPinMux(PORTA, PIN5_IDX, kPORT_MuxAlt4); /* PORTA5 (pin 55) is configured as MII0_RXER */
PORT_SetPinMux(PORTA, PIN9_IDX, kPORT_MuxAlt4); /* PORTA9 (pin 61) is configured as MII0_RXD3 */
PORT_SetPinMux(PORTA, PIN10_IDX, kPORT_MuxAlt4); /* PORTA10 (pin 62) is configured as MII0_RXD2 */
PORT_SetPinMux(PORTA, PIN11_IDX, kPORT_MuxAlt4); /* PORTA11 (pin 63) is configured as MII0_RXCLK */
PORT_SetPinMux(PORTA, PIN12_IDX, kPORT_MuxAlt4); /* PORTA12 (pin 64) is configured as MII0_RXD1 */
PORT_SetPinMux(PORTA, PIN13_IDX, kPORT_MuxAlt4); /* PORTA13 (pin 65) is configured as MII0_RXD0 */
PORT_SetPinMux(PORTA, PIN14_IDX, kPORT_MuxAlt4); /* PORTA14 (pin 66) is configured as MII0_RXDV */
PORT_SetPinMux(PORTA, PIN15_IDX, kPORT_MuxAlt4); /* PORTA15 (pin 67) is configured as MII0_TXEN */
PORT_SetPinMux(PORTA, PIN16_IDX, kPORT_MuxAlt4); /* PORTA16 (pin 68) is configured as MII0_TXD0 */
PORT_SetPinMux(PORTA, PIN17_IDX, kPORT_MuxAlt4); /* PORTA17 (pin 69) is configured as MII0_TXD1 */
PORT_SetPinMux(PORTA, PIN24_IDX, kPORT_MuxAlt4); /* PORTA24 (pin 75) is configured as MII0_TXD2 */
PORT_SetPinMux(PORTA, PIN25_IDX, kPORT_MuxAlt4); /* PORTA25 (pin 76) is configured as MII0_TXCLK */
PORT_SetPinMux(PORTA, PIN26_IDX, kPORT_MuxAlt4); /* PORTA26 (pin 77) is configured as MII0_TXD3 */
PORT_SetPinMux(PORTA, PIN27_IDX, kPORT_MuxAlt4); /* PORTA27 (pin 78) is configured as MII0_CRS */
PORT_SetPinMux(PORTA, PIN29_IDX, kPORT_MuxAlt4); /* PORTA29 (pin 80) is configured as MII0_COL */
Thanks. It solved the problem.
For some reason I enabled clock for all other ports except for PORTA.
 
					
				
		
 xiangjun_rong
		
			xiangjun_rong
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		hHi, Alex,
I guess that you do not enable the GPIO port clock, pls enable the GPIOA gated clock by setting the bit9 in SIM_SCGC5 register.
You can set the bit by the code if you use SDK2.0:
CLOCK_EnableClock(kCLOCK_PortA);
Before you set the PORTx_PCRy register, you have to enable the PORTx clock.
BR
XiangJun Rong