SDK transition and MCU transition

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SDK transition and MCU transition

852 Views
dotangoldberg
Contributor II

Hello,

1. I'm using FRDM64F for project evaluation include application and freeRTOS using SDK 2.0 IDE KDS 3.2

    A migration from SDK 2.0 to SDK 2.2 is needed

    Are there major differences between SDK2.0 and SDK2.2 drivers/middleware  

   (For example SPI,I2C,eDMA,...) and freeRTOS interface?

2. A transition from ev board MCU MK64FN1M0VLL12 to the target MCU MK24FN1M0VLL12 is needed

    Thus the freeRTOS based application from section 1 needs to be ported to MK24FN1M0VLL12

    It appears that SDK_2.2_MK24FN1M0xxx12 does not include freeRTOS code 

    While SDK_2.2_FRDM-K64F does include freeRTOS, why is the difference?

    What is the recommended way to do such a transition?

Thanks a lot,

Dotan

0 Kudos
Reply
1 Reply

722 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi dotan goldberg

About your questions;

1. No, there is not much difference between version 2.0 and version 2.2, so migration can be easily done. For changes you could check the release notes Document. you can find it in the path <SDK_2.2_K64F_path>\docs\MCUXpresso SDK Release Notes_MK64F12.pdf. chapter 9 include a list of "Change Log - Peripheral drivers"

2. SDK_2.2_MK24FN1M0xxx12 does include FreeRtos support. You have to add it in additional settings.

pastedImage_163.png

or if you have already selected your configuration, edit it in SDK Details

pastedImage_164.png

Hope this information could help you.

Have a great day,
Jorge Alcala

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply