SDK solution for MK20DX256VLH7 microcontroller.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SDK solution for MK20DX256VLH7 microcontroller.

2,298件の閲覧回数
arturoarteaga
Contributor II

Hi, I would like to know if there´s a SDK for MK20DX256VLH7 microcontroller . I´ve been searching about this but I haven´t found any. I would be grateful if someone knows any SDK solution for this microcontroller. Thanks a lot.

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,954件の閲覧回数
scottbrust
Contributor II

Is there still no official SDK for MK20DX256VLH7 CPUs?

Is creating a valid SDK for MK20DX256VLH7 as simple as changing #DEFAULT_SYSTEM_CLOCK in the SDK_2.2_MK20DX256xxx10\devices\MK20D10\system_MK20D10.h file?

Are all of the #defines in the MK20D10_features.h and MK20D10.h files accurate for the MK20DX256VLH7 CPU? 

0 件の賞賛
返信

1,954件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Scott,

i think the main difference of the two processor MK20DX256VLH7 and MK20DX256xxx10 is the clock frqeuency from software perspective, it is okay to reconfigure the #DEFAULT_SYSTEM_CLOCK.

Hope it can help you

BR

xiangjun rong

0 件の賞賛
返信

1,954件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Arturo,

I have found out that there is MK20DX256xxx10, i think you can download the SDK package based on MK20DX256xxx10, and modify the clock setting code so that the chip can run in 70mhz instead of 100MHz. You can click "Select Configuration"->"New configuration" to select the device.

BR

XiangJun Rong

pastedImage_1.png

0 件の賞賛
返信